Compensation tab
Use the settings on the
Compensation
tab to configure the compensation manual tuning parameters. Use the tab to:- Enter values for the friction and backlash compensation.
- Enter values for the system inertia and torque offset.
- Configure the Load Observer.
TIP:
To open the Compensation tab:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- In the lower left of theAxis Propertiesdialog box, clickManual Tune.
- In theMotion Consoledialog box, clickAdditional Tune > Compensation.
The
Compensation
tab includes these parameters.Parameter | Description |
|---|---|
System Inertia | Specifies a value for the system inertia. The values are in the range of 0 to Max Float. |
Torque Offset | Specifies a value for the torque offset in the range of -100 to 100. |
Friction Compensation | Specifies a value for the friction compensation. The values are in the range of 0 to Max Float. |
Friction Compensation Window | Specifies a value for the friction compensation window. The values are in the range of 0 to Max Float. |
Backlash Compensation Window | Specifies a value for the backlash compensation window. The values are in the range of 0 to Max Float. |
Load Observer Configuration | Shows the value for the Configuration on the Load Observer dialog box. Available values include:
|
Load Observer Bandwidth | Specifies a value for the load observer bandwidth. The values are in the range of 0 to Max Float. This parameter appears dimmed when Load Observer Configuration is set to Disable . |
Load Observer Integrator Bandwidth | Specifies a value for the load observer bandwidth window. This parameter appears dimmed when Load Observer Configuration is set to Disable . |
Provide Feedback