Select Tool File Dialog Box Overview
Use this dialog box to select an application (an .exe file) to add as a custom tool in the
Logix Designer
application. This dialog box includes the following parameters:
Parameter | Description |
|---|---|
Look in: | Select the directory in which to look for the application. |
Go To Last Folder Visited | Click this button to return to the previous folder you accessed. Note that this button appears dimmed until you have accessed more than one folder in this dialog box. |
Up One Level | Click this button to go up one level in the directory tree. Note that this button appears dimmed if you are at the top level of the directory tree. |
Create New Folder | Click this button to create a new folder in the current directory. |
View Menu | Click this button to display how the files display in this dialog box. The available options include:
|
File name: | Click the application listed in the Select Tool File dialog box that you wish to add as a custom tool in the Logix Designer application.The application you choose displays in the File name field. Note that you can click the arrow on this control to choose from a list of recently accessed applications. |
Files of type: | Executable Files (*.EXE) displays as a default in this field. |
Select | Click this button to add the selected application as a custom tool in the Logix Designer application. |
Cancel | Click this button to cancel the selection and close the Select Tool File dialog box. |
Provide Feedback