Driver and Path Configuration dialog box settings
Use the
Drive and Path Configuration
dialog box to manually enter a communications driver and path. The following are the Driver and Path Configuration
dialog box settings:
TIP:
- Configure ControlNet and DH+ drivers in the <RSLC> user interface or in theFactoryTalk Administration ConsoleforFactoryTalk Linx.
- Manually-entered drivers and paths do not appear in theWho Activedialog box. Drivers and paths appear wherever the current path normally displays, with the driver and path concatenated, such as AB_KTC-1\2,6,1,0.
Setting | Description |
|---|---|
Driver | Used to select from the list of running drivers in the communication software edition. |
Path | Enter the CIP path to a controller that Logix Designer uses when executing a Go Online , Upload , or Download command. The path also writes to any project.
NOTE:
For ControlNet and DH+ , construct the path starting from the communications module in the local chassis. Separate the number or addresses entered in each step with a comma. All numbers are decimal, by default. Enter any number other than an Ethernet/IP address in another base by using an IEC-1131 prefix ("8#" for octal, "16#" for hexadecimal). Ethernet/IP addresses are always dot-separated decimal numbers. |
Recent | Navigates to the Select Recent Communications Path dialog box, and select a recent saved path as the current communications path. |
Provide Feedback