Bit overlays are not currently supported by the Data Type Editor

It has been detected that, through the import command, you have created a structure that uses bit overlays. While it is legal to do this, the Data Type Editor will not support the modification of such structures, and therefore the view will be read-only.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal