A fault exists in standard control or safety task
Select
Yes
to confirm that you want to clear faults for these scenarios.A fault exists in standard control.
The controller keyswitch is in RUN, so clearing faults will restart Safety task and standard control execution.
A fault exists in safety task and in standard control.
The controller keyswitch is in RUN, so clearing faults will restart Safety task and standard control execution.
A fault exists in safety tasks .
Standard control is running, so clearing faults will restart Safety task execution.
A fault exists in safety task and in standard control.
A download is required to clear the Safety fault.
Provide Feedback