Configure PDI instructions
Use the
Advanced
tab to enable the use of the alternative source for PV in Maintenance.To configure Process Discrete Input (PDI) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
. - In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Open theAdvancedtab.
- Set the parameters:
- Substitute PV. When the check box is selected, the maintenance commands for selecting substitute PV and input PV are enabled.
- Follow PV target. Use the check box to allow the substitute PV to track the input target value, rather than using the maintenance substitute PV value.
- View the read-only parameters:
- Device state. When theLogix Designerapplication is online with the controller, the indicator displays the current device state, such as Off, Pulse on, or Out of service.
- Device issues. When theLogix Designerapplication is online with the controller, the indicator displays fault conditions, such as Feedback fault or I/O fault.
- SelectApply.
Provide Feedback