Edit an Add-On Instruction
Use these steps to edit an Add-On Instruction (AOI).
TIP:
The instruction must be unsealed. If the Add-On Instruction is a safety instruction, it cannot be safety locked or have a safety task signature.
To edit an Add-On Instruction:
- In theController Organizer, expand theAssetsfolder and double-click the AOI to open theAdd-On Instruction Definition Editordialog box.
- Configure parameters and local tags.
- Consider if any scan mode routines are necessary.
- Select theHelptab to view the instruction as it will appear in each language.
- Navigate to the Logic routine using theLogicbutton on theDefinition Editoror by selecting it in theController Organizer.TIP:You can only edit AOI logic when offline.
- To add an alarm for the AOI, right-click the instruction in theController Organizerand selectEdit Alarm Definitions. When theAlarm Definitions Listopens, right-click and selectNew Alarm Definition.You can also right-click a scalar tag or parameter of an AOI or a scalar member of a data type and selectAdd Alarm Definition.
Provide Feedback