Modify step tags or sequencing parameters using the Sequence Parameters Control

Select a step tag or sequencing parameter from the list on the Sequence Parameters Control to modify, disable or enable, force evaluation of, or view more information about the step tag or sequencing parameter.
TIP: To modify settings for tags and parameters, the external value for the tags and parameters must be set to
Read/Write
. Use the Tag Editor in the
Logix Designer
application to change the external value for a tag or parameter.
To modify a tag or parameter
  1. Select the tag or parameter.
  2. In the
    Value
    box, type the new value for the tag or parameter.
  3. To disable or enable a tag or parameter, select
    Expression
    and then select
    Disable Expression
    or
    Enable Expression
    . When you disable a tag or parameter, the disabled icon L5K_SILC_disabledExpression appears in the
    Expression
    box. To re-enable a disabled tag or parameter, select
    Expression
    and then select
    Enable Expression
    . When you re-enable a disabled expression, the disabled icon disappears from the
    Expression
    box.
  4. To force evaluation of a tag or parameter, select
    Expression
    and then select
    Force Evaluation
    . The
    Force Evaluation
    button is disabled when any of these are true:
    • The
      Equipment Sequence
      is in the IDLE state.
    • The controller is in Program mode.
    • The
      Equipment Sequence
      or its assigned task is disabled.
    • The
      Equipment Sequence
      is unscheduled.
      TIP:
      If a description is truncated, hover over the description to see the full description in a tool-tip.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal