Selected displays did not get published
If a web application that you published does not contain the expected displays, consider the following potential causes and remedies.
Publishing process incomplete
To publish a
FactoryTalk ViewPoint
application, you must complete the following steps:- Select aFactoryTalk Viewapplication
- Select graphic displays
- Publish graphic displays
Display not selected
On the
Select Displays to Web
screen, if the checkbox in the Web Enable
column is not selected, the display will not be published.- Verify the displays you wish to publish are selected before publishing.
Display deleted from application
If the display was deleted from the
FactoryTalk View
application, the display will not be published.- Verify the displays you wish to publish are in theFactoryTalk Viewapplication.
Publishing error or warning
A display or object may not be published if
FactoryTalk ViewPoint
generates an error or warning during the publishing process. All errors and warnings are shown on the publishing report.- To view the publishing report, on thePublish Displays to Webpage, clickView publishing report.TIP:For more information about the publishing process, see Knowledgebase Document ID: QA11471 - Process outline for publishingFactoryTalk View SEdisplays withinFactoryTalk ViewPoint.
Provide Feedback