Enable web application security
Web application security limits which user groups can view web application displays. If
enabled, permissions set in
FactoryTalk ViewPoint Administration
determine which actions user
groups can perform. Users will be required to sign in to access web applications.Users viewing a published web application when web application security is enabled must
refresh their browsers and sign in using their
FactoryTalk Directory
credentials.Web application security is not enabled until a new MER file is created and transferred to the operator terminal.
To enable web application security
- Open.FactoryTalk ViewPoint Administration
- From the navigation bar, selectSecurity Settings.
- (optional) If it is not selected, click theSecured Displaystab.
- Select theEnable Application Securitycheckbox.
- Select an application, area, or display from the list, and then select theWriteorViewcheckboxes to assign permissions to each user group.
- ClickSave.
Provide Feedback