Create an HTTPS binding for your site

For secure communications, HTTPS binding is recommended.
Prerequisites
  • Configure certificates on the
    PanelView™
    Plus 7 or
    PanelView Plus 6
    terminal and the client computers.
    For more information about setting up a server certificate for a Windows Embedded CE web server, see
    Microsoft
    documentation: How to Set Up a Server Certificate for a Windows Embedded CE Web Server.
    For more information about setting up a server certificate for a
    PanelView Plus 7 Performance
    Series B terminal, see
    PanelView Plus 7 Performance
    Terminals User Manual
    (publication 2711P-UM008).
  • If there is no user account in the
    User Account Manager
    on the
    PanelView Plus 7
    or
    PanelView Plus 6
    terminal, add a user account.
To create an HTTPS binding
  1. Start a web browser and in the browser's
    Address
    bar, enter the following URL, replacing
    computer_name_or_ip_address
    with the hostname or IP address of the
    PanelView Plus 7
    or
    PanelView Plus 6
    terminal:
    http://computer_name_or_ip_address/WebAdmin
  2. In the
    Enter Network Password
    dialog box, enter the user name and password specified in the
    User Account Manager
    dialog box, and press
    OK
    .
  3. On the
    Web Server Configuration
    page, click the
    Modify
    button after
    Default Web site
    .
  4. Click
    Configure the virtual directories on this Web site
    .
  5. On the
    Virtual Directory Configuration
    page:
    • Scroll down to
      /ftvp/
      and click
      Modify
      . On the
      /ftvp/Configuration
      page, in the
      SSL Configuration
      section, select the
      SSL Required
      checkbox and press
      Update
      .
    • (optional) Scroll down to
      /WebAdmin/
      and click
      Modify
      . On the
      /WebAdmin/Configuration
      page, in the
      SSL Configuration
      section, select the
      SSL Required
      checkbox and press
      Update
      .
      IMPORTANT:
      Before enabling SSL on the
      /WebAdmin/Configuration
      page, you must configure certificates on the terminal. If you didn't configure certificates, you will not be able to open the
      Web Server Configuration
      page.
      Self-signed certificates are not supported by this system. Use a certificate issued by a recognized Certificate Authority (CA) within your organization, or obtain one from a trusted commercial CA.
  6. Go to
    SSL Configuration
    page:
    1. Select the
      Enable SSL
      checkbox.
    2. In the
      Server Certificate Subject Line
      box, enter the common name specified in the certificate.
    3. Press
      Update
      .
  7. Press
    Restart Web Server
    to apply the changes.
After creating an HTTPS binding for your site, enter the following URL to connect to the web application, replacing
computer_name_or_ip_address
with the common name specified in the certificate:
https://computer_name_or_ip_address/FTVP
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal