Re-publish graphic displays

Re-publish all graphic displays to overwrite published displays even if their content has not changed. Because every selected display is published, re-publishing can take significantly longer than publishing.
If you upgrade the
FactoryTalk ViewPoint
software, the
Re-publish all selected displays
checkbox will be selected by default. Following an upgrade, you should re-publish the entire existing web application to ensure compatibility with the new software version.
To re-publish all displays
  1. On the
    Publish Displays to Web
    screen, click
    Select displays
    .
  2. In the
    Web Enable
    column, select whether each display should be re-published:
    • Selected - the display will be re-published
    • Cleared - the display will not be re-published
  3. In the
    Initial Display
    column, select which display will be shown when a user connects to
    FactoryTalk ViewPoint
    .
  4. Select
    Re-publish all selected displays
    .
  5. Click
    Publish displays
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal