ViewPoint trend does not display data
If a
FactoryTalk ViewPoint for Machine Edition
trend does not display any data, consider the following potential causes and remedies.No pen values selected
If all the check-mark boxes are unmarked, trend lines will not be visible.
- Verify at least one pen is selected in the Legend.
Trend paused
If the trend was paused before it received data, it may appear blank.
- Verify the trend is not paused.
Networking and communications failure
If networking and communications have failed on
PanelView Plus
, the FactoryTalk ViewPoint
server will be unable to communicate with the FactoryTalk View
Live Data servers.- View theFactoryTalk Viewapplication on thePanelView Plusgraphic terminal. If the same trend object is not displaying any data, the problem is not inFactoryTalk ViewPointbut at the lower levels such as the networking and communications.
Another typical symptom of networking or communications failure is partial or total wire-framing.
Provide Feedback