Loss of communication for graphic objects
If there is loss of communication for graphic objects in a display, consider the following potential causes and remedies.
Networking and communications failure
If networking and communications have failed on the host
PanelView Plus
terminal, the FactoryTalk ViewPoint
server will be unable to communicate with data servers.- View thePanelView Plusterminal hosting theFactoryTalk ViewPointserver and observe its behavior. If the same graphic objects also show a loss of communications, and then the problem is not inFactoryTalk ViewPointbut at lower levels such as networking and communications.
For troubleshooting these types of problems please refer to a number of articles in our knowledgebase that deal with causes and remedies for wire-framed graphic objects in the
FactoryTalk View ME
environment.Provide Feedback