Selected displays did not get published

If a web application that you published does not contain the expected displays, consider the following potential causes and remedies.
Publishing process incomplete
To publish a
FactoryTalk ViewPoint
application, you must complete the following steps:
  1. Select a
    FactoryTalk View
    application
  2. Select graphic displays
  3. Publish graphic displays
Display not selected
On the
Select Displays
screen, if the checkbox in the
Web Enable
column is not selected, the display will not be published.
  • Verify the displays you wish to publish are selected before publishing.
Display deleted from application
If the display was deleted from the
FactoryTalk View
application, the display will not be published.
  • Verify the displays you wish to publish are in the
    FactoryTalk View
    application.
Publishing error or warning
A display or object may not be published if
FactoryTalk ViewPoint
generates an error or warning during the publishing process. All errors and warnings are shown on the publishing report.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal