Objects on a display are not converted

If objects in the display are missing or do not behave as expected, consider the following potential causes and remedies.
FactoryTalk ViewPoint
does not support the object or all of its features
Some objects and features available in
FactoryTalk View Studio
are not supported in
FactoryTalk ViewPoint
. For a list of which
FactoryTalk View
objects are not supported in
FactoryTalk ViewPoint
, view the
FactoryTalk ViewPoint
Release Notes.
Unsupported objects or features generate an error or warning during the publishing process. All errors and warnings are shown on the publishing report.
  • To view the publishing report, on the
    Publish Displays
    page, click
    View publishing report
    .
Incorrect object properties or connections
If an object has incorrect properties or connections, it may not behave like other objects of the same time in
FactoryTalk ViewPoint
.
  1. Determine if other objects of the same type are working properly.
  2. Review the object properties and connections in
    FactoryTalk View Studio
    .
  3. Publish the displays again.
    TIP:
    For more information about
    FactoryTalk View
    features that are converted during publishing, see Knowledgebase Document ID: IN7597 -
    FactoryTalk ViewPoint
    :
    FactoryTalk View
    Object and Feature Support
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal