Enable web application security

Web application security limits which user groups can view web application displays. If enabled, permissions set in
FactoryTalk ViewPoint Administration
determine which actions user groups can perform. Users will be required to sign in to access web applications.
Users viewing a published web application when web application security is enabled must refresh their browsers and sign in using their
FactoryTalk Directory
credentials.
To enable web application security
  1. Open
    FactoryTalk ViewPoint Administration
    .
  2. From the navigation bar, click
    Security Settings
    .
  3. (optional) If it is not selected, click the
    Secured Displays
    tab.
  4. Select the
    Enable Application Security
    checkbox.
  5. Select an application, area, or display from the list, and then select the
    Write
    or
    View
    checkboxes to assign permissions to each user group.
  6. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal