Disable web application security
Web application security limits which user groups can view web application displays. If
disabled, users will not need to sign in to access web applications and all user groups may
view web application displays.
To disable web application security
- Open.FactoryTalk ViewPoint Administration
- From the navigation bar, clickSecurity Settings.
- (optional) If it is not selected, click theSecured Displaystab.
- Clear theEnable Application Securitycheckbox.
- ClickApply.
Provide Feedback