Disable administration security

Administration security limits which user groups can access
FactoryTalk ViewPoint Administration
. If disabled, users will not be required to sign in to use
FactoryTalk ViewPoint Administration
.
To disable administration security
  1. Sign in to
    FactoryTalk ViewPoint Administration
    with an account that has administration permissions.
  2. From the navigation bar, select
    Security Settings
    .
  3. (optional) If it is not selected, click the
    Administration
    tab.
  4. Clear the
    Enable Administration Security
    checkbox.
  5. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal