Re-publish all graphic displays
Re-publish all graphic displays to overwrite published displays even if their content has not changed. Because every selected display is published, re-publishing can take significantly longer than publishing.
If you upgrade the
FactoryTalk ViewPoint
software, the Re-publish all selected displays
checkbox will be selected by default. Following an upgrade, you should re-publish the entire existing web application to ensure compatibility with the new software version. To re-publish all displays
- On thePublish Displaysscreen, clickSelect displays.
- In theWeb Enablecolumn, select whether each display should be re-published:
- Selected - the display will be re-published
- Cleared - the display will not be re-published
- In theInitial Displaycolumn, select which display will be shown when a user connects toFactoryTalk ViewPoint.
- SelectRe-publish all selected displays.
- ClickPublish displays.
Provide Feedback