About automatic display synchronization

FactoryTalk ViewPoint
synchronizes its published web application with its
FactoryTalk View
application counterpart. Any changes to published displays are pushed from the
FactoryTalk View
application to the
FactoryTalk ViewPoint
web application.
Displays deleted from the
FactoryTalk View
application are automatically deleted in the
FactoryTalk ViewPoint
application. New displays added to the
FactoryTalk View
application are not automatically published to the
FactoryTalk ViewPoint
application.
Specify the automatic display synchronization settings on the
Server Settings
page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal