Sort alarms in alarm summary
Sort alarms in alarm summary to change the order in which alarms are shown. You can sort alarms by up to three alarm properties. By default,
FactoryTalk ViewPoint
only sorts alarms by date and time with the most recent alarm shown first.Refreshing the display resets it to the default sort options.
To sort an alarm summary
- In the alarm summary, select theSortbutton to open theSortwindow.

- From theSort alarms bylist, select an alarm property:
- None
- Ack
- State
- Date
- Message
- Priority
- Group
- Select a sort order option for the selected alarm property.
- Ascending- Show the alarm with the lowest value first.
- Descending- Show the alarm with the highest value first.
- (optional) From theThen bylists, select alarm properties and sort orders for second and third level sorts.
- ClickOK.
Provide Feedback