Shelve an alarm from the Details dialog box
If you have the permission to shelve an alarm in
FactoryTalk Security
, you can shelve an alarm from the Details
dialog box.
TIP:
Server-based events cannot be acknowledged or shelved.
To shelve an alarm
- From the alarm summary, select an alarm. TheDetailsdialog box shows.
- PressShelve ^.
- Enter the shelving duration (1-2147483647). The default shelving duration is 1 minute.
- (optional) In theCommenttext box, enter a comment. The comment is limited to 512 characters.
- PressShelve.
The result shows at the bottom of the alarm summary display.
Provide Feedback