Acknowledge an alarm from the Details dialog box
If you have the permission to acknowledge an alarm in
FactoryTalk Security
, you can acknowledge an alarm from the Details
dialog box.
TIP:
Server-based events cannot be acknowledged or shelved.
To acknowledge an alarm
- From the alarm summary, select an alarm. TheDetailsdialog box shows.
- Press theAcknowledge ^.
- (optional) In theCommenttext box, enter a comment. The comment is limited to 512 characters.
- PressAcknowledge.
The result shows at the bottom of the alarm summary display.
Provide Feedback