Cross Reference form
How do I open the Cross Reference form?
From the tool bar, click
or select
or select Cross Reference
from the Tools Menu.Use the
Cross Reference
form to specify the tag or text string to be searched for, the location, and components to be searched and then show the location and components in a spreadsheet form.Use the Cross Reference function to search for tags and text strings in the following product component types:
- Global Connections (Machine Edition only)
- Tag Database
- Graphic Displays
- Global Objects
- Parameters
- Alarm Setup (Machine Edition only)
- Macros
- Datalog
- RecipePro+
Provide Feedback