Export configuration

Use the
Export configuration
dialog box to export the entire data log configuration in a CSV file, including all log groups, tags, and trigger properties. It always exports the entire configuration no matter which group is selected.
To export the configuration, specify the CSV file name and its path, and then select
Export
. If a file with the same name already exists in the target folder, it will be replaced by the new CSV file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal