Examples: DisplayClientOpen
DisplayClientOpen Client1.cli
Opens a client that is on the local drive and in the path.
DisplayClientOpen C:\DST\Client1.cli
Opens a client that is on the local drive but not in the path.
DisplayClientOpen J:\DST\Client1.cli
Opens a client that is on a network drive and not in the path.
Provide Feedback