EventOn

Starts running the specified event file.
Syntax
EventOn
<component>
where
<component>
is a relative or absolute reference to an Events file. If the file name has a space in it, enclose the name in double quotes.
Remarks
Select the Event Detector check field in the Components tab of the HMI server's Properties dialog box and choose a file, to have that event file started automatically when a project is started.
This command can be issued from the
FactoryTalk View SE
Client,
FactoryTalk View Studio
, or HMI server, but is always run on the HMI server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal