DerivedOn

Starts running the specified derived tag file.
Syntax
DerivedOn <
component
>
where
<component>
is a relative or absolute reference to a Derived Tag file. If the file name has a space in it, enclose the name in double quotes.
Remarks
Check the Derived Tags check box in the Components tab of the HMI server's Properties dialog box and choose a derived tags file, to have that file started automatically when a project is run.
This command can be issued from the
FactoryTalk View SE
Client,
FactoryTalk View Studio
, or HMI server, but is always run on the HMI server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal