Unpin
Unpins the pinned display from top. The display remains on top until it is replaced by a
Replace
display. Without a parameter, the command unpins the active display.Syntax
Unpin
[*
]where
*
unpins all pinned displays.Remarks
This command applies to the
On Top
display only.This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a FactoryTalk View Studio
or HMI Server.Provide Feedback