PushBack

Moves the specified file behind all other windows.
Syntax
PushBack <
display
>
where
<display>
is a relative or absolute reference to a graphic display. If the file name has a space in it, enclose the name in quotes.
Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a
FactoryTalk View Studio
or HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal