Equal
Equal (EQ or ==)
Compares the two values and returns a 1 (true) if they are equal, or a 0 (false) if they are not equal.
FactoryTalk View uses a double equals sign (==) as an operator because the single = is used elsewhere in the system as the equal command.
Provide Feedback