Search
FactoryTalk View SE Help
Bitwise AND
Bitwise AND (&)
Returns an integer with a bit set to 1 if both of the corresponding bits in the original numbers are 1. Otherwise, the resulting bit is 0.
Functions and operators
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal