Format expressions
Expressions can have tabs, new line characters, and multiple spaces. This lets you format an expression so that it is easier to understand. Press
Ctrl
+ Tab
to insert a tab in an expression in the animation dialog box in graphic displays.For example, you can align the else with the appropriate If so the logic is easier to understand. You can also remove extra spaces and line breaks to make maximum use of the editor space.
TIP:
Do not allow tag names, keywords, function names, or function arguments to span more than one line.
Provide Feedback