Use objects of Graphics Libraries
You can easily create your displays by using objects of the Graphics Libraries.
To use objects from the Graphics Libraries:
- In FactoryTalk View Studio, open the graphic display you intend to put the objects in.
- Under the HMI server, expandGraphics>Librariesand double-click the library component containing the objects you want to use.
- Drag the objects from the library display to your graphic display.TIP:Any animation that has been attached to an object will be carried along with it.
Provide Feedback