FactoryTalk View SE Website Setup tool
How do I open
FactoryTalk View SE
Website Setup tool?
Select
Start > Rockwell Software > FactoryTalk View SE Website Setup
.FactoryTalk View SE
(Network Distributed) installs IIS (Internet Information Services) to move information between HMI servers and client computers. When FactoryTalk View SE
is installed, it creates a default website on the HMI server computer.If your application requires a higher level of security than the level provided by the default website, use the
FactoryTalk View SE
Website Setup tool to do one of the following:- Enable the HTTPS protocol over the default website.
- Create a custom website on an HMI server computer using a private TCP port number (49280) instead of the default port number (80).
If either one of them is enabled, it's recommended to disable the other.
Provide Feedback