Graphic display XML file example
The following XML file example shows a Site Edition graphic display with a few objects on it, including a text object, a numeric display object, a numeric input enable object, and a group containing two rectangles, one of which is animated. Not all the possible properties for these objects are shown in this file. Any objects or properties that are not listed will not be modified when the file is imported.
<?xml version="1.0" encoding="UTF-8"?> <gfx xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xsi:noNamespaceSchemaLocation="Gfx-SE4.xsd"> <displaySettings displayType="replace" backColor="white" width="640" height="480"/> <text name="Text1" height="16" width="87" left="69" top="42" caption="Pump House 1"/> <numericDisplay name="NumericDisplay1" height="44" width="104" left="234" top="150" borderStyle="raisedInset"> <connections> <connection name="Value" expression="{[clx1]Count_Up[0]}"/> </connections> </numericDisplay> <group name="Group1" wallpaper="false"> <rectangle name="Polygon1" height="35" width="53" left="378" top="40" visible="true"/> <rectangle name="Polygon2" height="35" width="56" left="428" top="85" visible="true"/> <animations> <animateVisibility expression="system\BlinkFast" expressionTrueState="visible"/> </animations> </group> <numericInputEnable name="NumericInputEnable1" height="55" width="80" left="57" top="142" keyAssignment="F1"> <caption fontFamily="Arial" caption="Stop"/> <connections> <connection name="Value" expression="{[clx1]n7[0]}"/> </connections> </numericInputEnable> </gfx>
Provide Feedback