Batch import file
A batch import file is:
- In XML format
- Used to import multiple XML files into multiple graphic displays in one step
- Created automatically when you do an export operation and namedBatchImport_<HMI Project name>.xml
- Created in the same directory as the XML files exported for each graphic display, that is, the location specified in theExport Folderdialog box of the Graphics Import Export Wizard
Provide Feedback