Trend is missing data when scrolling
Problem
Data outside of the visible trend chart area is lost. When you scroll backward or forward, data is missing.
Cause
The trend object stores a limited number of extra data points in addition to those shown. You can configure the amount of extra data stored in a buffer.
Solution
On the Display tab, configure the
Buffer for extra data
option to hold more records per pen.Provide Feedback