Trend is missing data points
Problem
Some transitions are skipped and corresponding data points do not show on the trend.
Cause
The trend object might be polling and updating with data periodically, rather than on change. For example, if data values change every second but the
Refresh Rate
is set to once per minute, changes in data will be missed.Solution
On the General tab, change the chart update mode to
On Change
, or increase the speed of the Refresh Rate
.Provide Feedback