Range on trend chart is not as expected
Problem
The range of values shown on a trend chart is not what you expect it to be. For example, the pen's minimum and maximum values are configured as 1 and 100, but the chart shows a range from -50 to 50.
Cause
The trend object offers a variety of range options, controlled by options set on the Y-Axis tab. The pen's minimum and maximum values might fall outside of the specified range or outside of the specified scale configured on the
Y-Axis
tab.Possible solutions
On the
Y-Axis
tab, check the following:- WhichMinimum / Maximum Valueoption is selected.
- WhichScaleoption is selected.
Provide Feedback