Pen is missing from the trend chart
Problem
A configured pen does not show on the trend.
Possible solutions
On the
Pens
tab, make sure that:- TheVisibleoption isOn.
- The pen line color is not the same color as the chart's background color specified on the Display tab.
- The pen has a marker assigned, if theData Point Connectionoption on theDisplaytab is set toShow Only Markers.
On the Y-Axis tab, check the chart range, as defined by the
Minimum / Maximum Value
options. If the pen's data is all outside of the specified range, the pen's trend line draws at the top or bottom of the chart, where it might not be noticeable.Provide Feedback