Numbers show as decimals

Problem
Numbers on the trend chart show as decimals, even though you have selected
Octal or Hexadecimal
as the
Chart Radix
setting on the Display tab.
Solution
On the Y-Axis tab, change the number of decimal places to zero. If the number of decimal places is set to anything other than zero, numbers cannot be accurately converted to octal or hexadecimal.
To provide accurate data, the trend shows the numbers as decimals.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal