Set up general options for a Pause Pen button
Use the
General
tab of the Pause Pen Button Properties
dialog box to set up general options for a Pause Pen
button.To set up general options for a Pause Pen button
- In theGraphics Displayeditor, double-click thePause Penbutton to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options as needed.
Provide Feedback