Set up general options for a Next Pen button

Use the
General
tab of the
Next Pen Button Properties
dialog box to set up general options for a
Next Pen
button.
To set up general options for a Next Pen button
  1. In the
    Graphics Display
    editor, double-click the
    Next Pen
    button to open its
    Properties
    dialog box.
  2. Click the
    General
    tab.
  3. Specify the options as needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal