Runtime fonts
Licensed fonts for
PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, and PanelView Plus CE
terminals are supplied on the Accessories or Fonts CD. Users are requested to use only the fonts provided on these CDs with their terminals. Download the fonts to the terminal using ME Transfer Utility.FactoryTalk View ME Station
also supports font linking for PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, and PanelView Plus CE
terminals. Use the Font Linking
menu in the Terminal Settings
dialog box to select a base font and to link another font to the base font. Both the base font and the linked font must be loaded on the terminal.
TIP:
Bold or italic text that looks correct on the desktop computer may be truncated on the
PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, and PanelView Plus CE
terminal. This is because, by default, only plain fonts are installed on the terminals. If you need bold or italic fonts for your application, download the bold/italic versions from the Fonts CDs.Provide Feedback