Product support
If you cannot find the answer to your question in the documentation or on the Internet, contact
Rockwell Automation
.Customer Support Telephone — 1.888.382.1583 or 1.440.646.3434
When you call, it is recommended that you be at your computer and ready to provide the following information:
- The product’s serial number and product key, which are printed on the Activation Certificate enclosed with the product software DVD
- FactoryTalk Viewversion number
- FactoryTalk Services Platformversion number
- FactoryTalk Linxversion number
- The type of hardware you are using
- The names of otherRockwell Automationproducts installed on the computer
- The exact wording of any messages shown on the computer
- A description of what happened and what you were doing when the problem occurred
- A description of how you tried to solve the problem
To view the list of installed add-ons and updates
- In FactoryTalk View Studio, selectHelp > About FactoryTalk View Studio.
- To view the list of installed add-ons, clickAdd-Ons.
Provide Feedback