Modify a user properties at runtime
Use the
Change User Properties
dialog box to modify a user properties at runtime.To modify a user properties at runtime
- Press theChange User Propertiesbutton to open theChange User Propertiesdialog box.
- PressSelect Userto open theFactoryTalk User Selectiondialog box.
- PressUporDownto select a user or group.TIP:TheFactoryTalk User Selectiondialog box only shows the users already configured inFactoryTalk Directoryand packed in the application.
- Press theSelectbutton, orEnter
on the external keyboard to select the user. - PressPropertiesto set the following options if needed, and clickOK. The advanced settings are set toNoby default.
- User must change password at next logon
- User cannot change password
- Password never expires
- Account is disabled
- PressChangeto close the dialog box and save the changes.
The operation status shows in the
Result
box.Provide Feedback