Set up general properties for a Change User Properties button
Use the
General
tab of the Change User Properties Button Properties
dialog box to set up how a Change User Properties
button looks.To set up general options for a Change User Properties button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
Once you set up the options on the
General
tab, click the Label
tab to specify a caption or image for the button.Provide Feedback