Use the Unlock User Account dialog box
Use the Unlock User Account dialog box to unlock a user account at runtime.
TIP:
When a
FactoryTalk
user exceeds incorrect password login attempts, the user account will be locked. When the user account is locked, the user cannot log in to the system even with correct password before the user account is unlocked.To unlock a user account at runtime
- Press theUnlock Userbutton to open theUnlock User Accountdialog box.
- PressSelect Userto open theFactoryTalk User Selectiondialog box.
- In theSelect Userfield, press theUporDownkey to select a user account.
- Press theSelectbutton, orEnter
on the external keyboard to select the user account. - Press theUnlockbutton, orEnter
on the external keyboard to unlock the selected user account.
The operation status shows in the
Result
box.
TIP:
- You can adjust the account lockout threshold and account lockout auto reset settings in FactoryTalk Security Policy Settings. For more information on FactoryTalk Security Policy Settings, refer to "Setting up security policies" inFactoryTalkHelp.
- You cannot use theUnlock Userbutton to unlock a Windows-linked user. Only a Windows Domain administrator can unlock a Windows-linked user from a domain computer.
Provide Feedback